Part Number: TUSB2E22
Other Parts Discussed in Thread: TUSB2E11,
Hi Team,
May I check the detail EQ value of different compensation level? Is it the same as the TUSB2E11 with two channel?
Best Regards,
Jaden Yue
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jaden,
The TUSB2E11 has 3 GPIO pins to select various EQ settings.
The TUSB2E22 has 2 GPIO pins (EQ0/EQ1). So, the TUSB2E11 has a greater ability to be fine-tuned.
I will follow to find if the maximum compensation and minimum compensation is the same between the two.
Regards,
Nicholaus
Hi Jaden,
Sorry, I meant to respond yesterday. You can view the dB loss values for various signal conditioning settings in the TUSB2E11 datasheet in the register map, but it doesn't show data for pin-strap mode. The TUSB2E22 is only pin-strap. It is taking a while to find this information.
Regards,
Nicholaus
Hi Jaden,
Here are the signal conditioning values for the TUSB2E22.
|
EQ0 pin |
EQ1 pin |
Compensation Level |
eUSB Amplitude |
eUSB Rx EQ |
eUSB Tx Pre-Emphasis |
|
0 |
0 |
Level 0 |
420mV |
0.81dB |
0.67dB |
|
1 |
0 |
Level 1 |
420mV |
1.46dB |
1.29dB |
|
0 |
1 |
Level 2 |
460mV |
2.55dB |
2.41dB |
|
1 |
1 |
Level 3 |
500mV |
3.13dB |
3.41dB |
Regards,
Nicholaus
Hi Jaden,
What customer/project is this for? It may be helpful to add [Project][Customer] to the E2E issue.
Regards,
Nicholaus
Hi Jaden,
Let me know this information about project/customer when you get a chance.
Are there any other questions about this issue?
Thanks,
Nicholaus