Part Number: TLIN1029A-Q1
Other Parts Discussed in Thread: ESD751-Q1, ESD1LIN24-Q1
Hello team,
My customer is asking me about the below item. Can you tell me your opinion?
<Question>
- Is it OK to place a chip varistor between LIN(pin6) and GND?
<Spec of the varistor>
Maximum permitted circuit voltage: 26V
Varistor Voltage Range: 30.6 to 37.4V
Varistor Voltage (Tolerance): 33V
Max. Specified capacitance: 100pF
<Background>
- My customer is doing a surge test based on IEC61000-6-2. The surge voltage is applied to LIN(pin6).
- They tried 2 tests. (Place of 1. Zener diode, 2. TVS diode: ESD751-Q1 and ESD1LIN24-Q1)
- But the tests was fail. Pin 6 was broken by the surge voltage. So they are considering to apply a chip varistor.
Best regards,
Shotaro