Part Number: SN55189A
Other Parts Discussed in Thread: MC1489A, , SN75C189A
Hi,
We are planning to replace MC1489AN with SN55189AJ as MC1489AN is in LTB.
MC1489AN's operating temperature range is 0°C to 70°C and SN55189AJ's operating temperature range is –55°C to 125°C.
The Positive-going input threshold voltage is not given at 0°C to 70°C for the MC1489AN (1.55V to 2.25V) and –55°C to 125°C for the SN55189AJ (1.30V to 2.65V) part. I wanted to know if SN55189AJ is being operated at 0°C to 70°C, will it have same value as MC1489AN?
The Negative-going input threshold voltage is not given at 0°C to 70°C for the MC1489AN (0.65V to 1.25V) and –55°C to 125°C for the SN55189AJ (0.35V to 1.6V) part. I wanted to know if SN55189AJ is being operated at 0°C to 70°C, will it have same value as MC1489AN?
Thank you,
Komal Garlapati.