Other Parts Discussed in Thread: TCAN3413, SN65HVD233, TCAN332, TCAN3403-Q1, TCAN3404-Q1, TCAN3404
Hello,
I am looking for a new CAN transceiver for a new from scratch design. Since I last looked at CAN many years ago, there are higher speed devices and devices that run on 3.3V that are interesting.
TCAN3414 is an example. It appears to run solely off a 3.3V supply and support up to 8Mbps CAN FD. I have the following questions:
- The datasheet specifically says "up to 8 Mbps operation in simpler networks is possible with these devices." There is no further mention of what this exactly means. What is the threshold on a simpler network vs less simple networks? Can this chip work at 5Mbps for all other networks then?
- I don't have a 5V supply in my system so using 3.3V is intriguing to me. Section 8.3.1.4 of the datasheet suggests the only difference between a 3.3V device and a 5V device is the recessive common mode voltage, but it seems that is still within the ISO CAN spec. However, there are much fewer 3.3V systems on the market. I am curious if there are other tradeoffs that aren't mentioned here? Is it just a legacy thing, or if I care a lot about performance, I should consider 5V?
- I have read app note SLLA337 and I am trying to weigh the cons of interoperability between 3.3V and 5V as well. If we have a common ground system with two CAN nodes talking to each other (one at 3.3V and one at 5V), it seems to me that there will be common mode current flowing from the 5V node to the 3.3V node in both the recessive state and states where 5V is trying to dominate. As we alternate between those two states and the 3.3V dominant state, the common mode current would alternate. I presume there is voltage division going on inside the chip to allow for a wide common mode range. Does that mean these common mode currents are small? Or is this a valid concern?
Thanks!