Part Number: TS3USB221E
Hi team,
Customer is considering to use VBUS (for preferred port) as S.
Is there any problem?
Especially concerned about the voltage rating and signal rise/fall time.
Best regards,,
Goto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3USB221E
Hi team,
Customer is considering to use VBUS (for preferred port) as S.
Is there any problem?
Especially concerned about the voltage rating and signal rise/fall time.
Best regards,,
Goto
Hi Goto-san,
I believe this should be a fine application, yes. The absolute max for the control pins is 7V, and we have no defined max in the recommended operating conditions, so I see no issue there. Using VBUS to control the S pin should not affect the signal rise/fall time going through the mux. Is the device being powered by pulling VBUS down to 3.3V, or is it being powered by an external 3.3V?
Thanks,
Ryan
Are there any other questions here? If not, I will close.
Thanks,
Nicholaus