Part Number: DS90UH948-Q1
hello:
The customer has currently developed a display screen product based on the TI UH948 deserializer, which uses UB949 for host debugging. They have the following questions that need support and answers regarding this project:
1. Please provide a register instruction manual for UH949/UB949/UH948/UH948;
2. Is the configuration of UB948 and UH948 compatible, that is, there is no need to change the configuration for the illuminated screen? Can UB949 and UH948 be paired for configuration?
3. The main purpose of choosing UH948 this time is to support HDCP function on the screen. HDCP is an encryption function, which we understand as pure software. As a pure hardware screen manufacturer, does the customer still need to test this HDCP function?