Part Number: SN65DSI84
Hi team
We have a device with a LVSD connector that will connect to three types of LCD panel.
- The First type of LCD panel can work with the frequency in range of 60MHz to 75MHz;
- The Second type of LCD panel can work with the frequency in range of 60MHz to 87.5MHz;
- The third type of LCD panel can work with the frequency in range of 69.22MHz to 73.9MHz;
Currently the REFCLK pin is connected to a crystal oscillator that can generate 26MHz clock.

The REFCLK_MULTIPLIER is only support 1 ~ 3, so for 26MHz Ref clock, the REFCLK_MULTIPLIER should be set to 3 that can closely match the LCD panel's frequency, and the actual frequency will be 78MHz, this frequency will exceed the some panel's max frequency(75MHz).
SO, if we want to support the three types panel with the external crystal oscillator , how can we select the output clock of the external crystal oscillator ?
Snow
Best regards