Part Number: THVD2410
Hi
We are planning to use THVD2410 as a replacement to MAX3440EESA+ without any change to the software. There is some pin difference between the two. Since , we do not intend to change the software , can i short the DE and RE pin (MAX3440 has a single RE/DE pin).
1) Is it allowed to short RE and DE. Will there be any negative impact.
2) If both of these pins are shorted and microcontroller pin is undefined, would it cause any issue? Because DE pin will be pulled up 2Mohm and RE pin will be pulled down by 2Mohm. Is it better to add a strong pull down so that the pin will be at defined state in default.
Please let me know.