Part Number: TCA9803
Other Parts Discussed in Thread: PCA9306, LSF0102

Hello, in the figure, the 3.3V/1.8V master requires communication with four 1.2V slaves through I2C buffer. Is there any suitable scheme to recommend
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
the a sides can not connected to master,because the master is 3.3V /1.8V,the slave is 1.2V, is there any other recommendation
There is an important point here, that is, the B end is the current source, not allowed to pull up, but the B end is to pick up the customer has designed the board, this I can not change
For level shifting, you could use the PCA9306/LSF0102 (it is not a buffer but a passive switch; it has the restriction that Vref_B must be larger than Vref_A, but the I/O voltages can be any voltage not below Vref_A).
For our application here,What are the advantages and disadvantages of PCA9306 compared with TCA8306?