Part Number: SN65DP159
We are building a video device where the source of the output signal is an Altera FPGA.
The problem is out put on the 4 N channels is flat - meaning it is not the inverse of the corresponding P.
Pins are
21 OUT_CLKN
22 OUT_CLKP
24 OUT_D0N
25 OUT_D0P
26 OUT_D1N
27 OUT_D1P
28 OUT_D2N
29 OUT_D2P
All 4 P lanes produce what appears to be correct signaling. All 4 N lanes produce no signal. When polarity is flipped, The situation remains the same. Meaning P lanes are correct N lanes are not.
This would lead me to believe there is a configuration issues versus a schematic error.

Any help or suggestions greatly appreciated.