This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044AV-Q1: Do you have any CAN transceiver which can replace MCP2562-E/SN?

Part Number: TCAN1044AV-Q1

Hello guys,

One of my customers is looking for TI CAN transceiver which can replace MCP2562-E/SN.

Microchip
MCP2562-E/SN
https://ww1.microchip.com/downloads/en/DeviceDoc/20005167C.pdf

This device has standby mode and Vio pin. Also package is SOIC(TI package code is "D").

I think that TCAN1044AVDRQ1 could be used.
But MCP2562-E/SN has High performance ESD performance which meets IEC61000-4-2 up to +/-14kV.

I have the following questions. Could you please give me your reply?

Q1.
Does TI have any CAN transceiver which can replace MCP2562-E/SN except TCAN1044AVDRQ1?

Q2. 
Does TI have any CAN transceiver which has high performance ESD performance which meets IEC61000-4-2 up to +/-14kV?

Your reply would be much appreciated.

Best regards,
Kazuya.

  • Hi Kazuya,

    Q1.
    Does TI have any CAN transceiver which can replace MCP2562-E/SN except TCAN1044AVDRQ1?

    TCAN1044AV is the choice. It's a pin-to-pin replacement with standby mode. Another 8-pin device will be TCAN1057A however it has an S pin for silent mode control which is different from MCP2562-E/SN.

    Q2. 
    Does TI have any CAN transceiver which has high performance ESD performance which meets IEC61000-4-2 up to +/-14kV?

    As part of our certification testing, we don't perform IEC61000-4-2 air gap discharge testing, but we do air gap discharge based on the J2962-2 specification. This ESD testing is a derivative of the IEC61000-4-2 ESD test, but it uses a system approach rather than a singular device, and the RC network in the ESD striking tool is 2k ohms and 330pF, rather than 330 ohms and 150pF in the IEC61000-4-2 testing. In the J2962-2 testing, our device survives to 15kV.

    See the test report below:

    https://sps16.itg.ti.com/sites/trx/TRXField/SiteAssets/Product%20Information/CAN/2%20-%20Product%20Information%20-RTM/TCAN1044A(V)-Q1%20and%20TCAN1057A(V)-Q1/EMC%20Test%20Reports/J2962-2/TCAN1044A%20J2962-2%202020-700%20Texas%20Instruments%20Summary%20of%20Testing.pdf

    Regards,

    Sean

  • Hi Sean,

    Thank you very much for your reply.

    But I couldn't access the URL.
    Could you please attach the test report to this thread?

    Thank you again and best regards,
    Kazuya.

  • Hi Kazuya,

    The link posted is to our internal site, so it's only accessible to TI employees. I can share the test report with you directly via email. If you give us permission here, we can forward this report to the email address you have linked to your E2E account.

    If you would prefer a different address, please send Sean or myself an email requesting the J2962 test report for TCAN1044A. You can find my contact information by clicking on my E2E name. 

    Regards, 
    Eric Schott