Part Number: DP83826I
Hello,
Let me confirm which information is correct.
According to datasheet (Rev G), you have described as shown below for strap configuration. 
However, according to schematic of EVM (https://www.ti.com/jp/lit/ug/snlu262a/snlu262a.pdf), it seems that "2.49k" ohm is used to perform "PD"(Pull Down).
According to above datasheet information, I believe that "1.5k ohm" should be used in this case. However EVM shows oppsition.
Q1. Which one is correct ?
And also, in case of EVM, it seems "ENHANCED mode" is set as default. (This pin is "floating" state.)
So, default value of PHY address is "000". However, you set these pin as "PD" even though it seems state of these pins are internal pull down.
Q2. Why did you add external pull down to these pins ?
Best Regards,