This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043-Q1: performance check

Part Number: TCAN1043-Q1

Hi Team,

Customer is considering TI TCAN1043ADMTRQ1 and TCAN1044AVDRBRQ1 to replace NXP. But they wonder if we can meet below requirement?

 Looking forward to your kindly reply!

Symbol

CAN clock

Tq

Tq

TSJW

TSEG2

TDC(Transmitter delay compensation)

Bit type

SP

SSP

per bit time

(ns)

(Tq)

(Tq)

Bit rate 500kbps

10M

20

100

4

4

/

normal

80%

/

Bit rate 500kbps

20M

40

50

8

8

Bit rate 500kbps

40M

80

25

16

16

Bit rate 2Mbps

20M

10

50

3

3

Enabled

data

70%

70%

Bit rate 2Mbps

40M

20

25

6

6

Bit rate 2Mbps

80M

40

12.5

12

12

 Thank you!

Marc