Part Number: SN65LBC180
Other Parts Discussed in Thread: THVD1512, THVD1552
I still have some questions about RS485 (SN65LBC180DR),
- Whether termination is required ? If yes, What is the value and whether it is required for both the ends ?
- Since we observe different state of DE and RE pin ?What should be the standard state of DE and RE pin to work in half and Full Duplex ?
| Full Duplex | Half Duplex | |||
| DE | RE | DE | RE | |
| Transmit | High | Low | High | Low |
| Receive | High | Low | Low | Low |