Hi Team,
I am using below mentioned poc circuit. I have some questions regarding that poc circuit.
My requirement for PoC circuit is:
Current= 500mA
Temperature rating= -20'C to 55'C
Frequency: 25MHz to 2.1GHz

Query 1: My current requirement is 500mA. Will this circuit support my current requirement for the required temperature range? if No please share suggesting which circuit i need to follow to match my requirements
In the mentioned document they said this circuit will work on only 250 mA on 105 C temperature rating.

Component used part no.:
FB1, FB5, FB6= BLM18HE152SZ1D
L1= ADM32FSC-100M
R4= CRCW06034K02FKEA
C40, C43 = GRM155R71E104KE14J
C41, C42 = GRM188R6YA106MA73D
Please let me know if you have any query.