Hi, due to protection and power restrictions I have 2 x 5V lines. 1 that goes directly to supply the main MCU and the other is a switching reg that is for my transceivers. All of the documentation I see if for different voltages for VIO implementation, can I use if with the 5V from regulator going to VCC and the 5V that supplies the MCU going to VIO to make sure it matches MCU voltage exactly?
Also, should I change my switching regulator to 5.1V instead of 5V to make sure VCC is over VIO?
Thank you!