Part Number: DS250DF230
Other Parts Discussed in Thread: DS250DF210, USB2ANY,
- Issue : 25G port work abnormal
- Behavior description : No any connection indication when plug SFP module between SUT and server side. Furthermore, we also find the register 0x02 will keep change between 0x98,0x80,0x01. So Please kindly help to comment.
- Environment setting
- SW version: Sig Con Architect Version : 2.0.0.8 + DS250DF210 Updater.
- HW connection tools: Dongle – TI USB2ANY
- SUT PCB material : EM-390+RTF
- Document reference:
- Programmer’s Guide – DS250DF230
- Chapter 5.2 Front-Port Egress (i.e. Host-to-Module)
- Chapter 5.3 Front-Port Ingress (i.e. Module-to-Host)
- Debug direction
- Step 1 - Using TI- GUI interface to check CDR could be locked or not by using loop back connection.
- Result : Follow Chapter 5.2 and 5.3 setting, TX(Host-to-Module) : CDR could be locked, but RX(Module to Host) no response
- Step 2 - Checking TX(behind the DS250DF230) Eye diagram could meet 25G criteria or not ?Checking : Using Tx FIR/VOD tool with test pattern - PRBS 9 to fine tune parameters, Pre Cursor Tap/ Main Cursor Post.
- Result :
- TX(I2C addr:0X27/4E) – Channel 0
- Pre Cursor Tap - -6
- Main Cursor - +20
- Post Cursor Tap - +0
- TX(I2C addr:0X27/4E) – Channel 1
- Pre Cursor Tap - -4
- Main Cursor - +18
- Post Cursor Tap - -4
- Step 1 - Using TI- GUI interface to check CDR could be locked or not by using loop back connection.
- Architecture Block Diagram

- Tx Fine tune result
- TX(I2C addr:0X27/4E) – Channel 0

-
- TX(I2C addr:0X26/4C) – Channel 1