Part Number: TPD4S009
Other Parts Discussed in Thread: TPD4S012
Wanted TPD4S009DRYR , ordered TPD4S012DRYR because I thought it was TPD4S009DRYR 's T+R version manufacturing #.
What are the differences?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there,
Here is a quick comparison table of the specifications for each of these devices:
| TPD4S009DRYR | TPD4S012DRYR | |
| Vrwm (V) | 5.5 | 5.5 |
| Package Type | USON | USON |
| Nominal Package Size (L x W) (mm) | 1.45 x 1.0 | 1.45 x 1.0 |
| Bi-/uni-directional | Uni-directional | Uni-directional |
| Number of Channels | 4 | 4 |
| IO Capacitance (typ) (pF) | 0.8 | 0.8 |
| IEC 61000-4-5 (A) | 2.5 | 3 |
| IEC 61000-4-2 Contact (kV) | 8 | 10 |
| Max Leakage Current (nA) | 100 | 500 |
Even though these devices are in the same package, they do have different pin outs. Please see the below diagrams on the pin layout of each device:
TPD4S009:
TPD4S012:

Please let me know if you have any questions!
Best Regards,
Josh Prushing