Part Number: TPD1E0B04
Other Parts Discussed in Thread: ESD441
Hello,
Why there are Common Anode and Common Cathode ESD bidirectional ESD diodes,on what basis should we choose them ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sobin,
In the bi-directional layout, there is not a functional difference between these two configurations. A bi-directional common anode should function the same as a bi-directional common cathode. The only difference I am aware of is the process used to create the die could potentially optimize certain specifications in one of these configurations.
So, in short, the only basis for choosing between these bi-directional configurations is any specifications that fit your application best.
Please let me know if you have any additional questions!
Best Regards,
Josh Prushing
Hi Josh,
Thanks for answering the query. Do we need to add any series resistance to limit current through the ESD diodes.
Regards,
Sobin
Hi Sobin,
In order to address this, I would need to know a little bit more about your application. In general, we do not see a need to limit current through the ESD diode. Below is a TLP graph from one of our devices, ESD441. This device can handle a good amount of current, the voltage will simply just increase as the current does.

This increased voltage can be detrimental to your downstream circuitry depending on the absolute maximum voltage of the device you are trying to protect. Generally, with the knowledge of the device/interface, we have recommendations that take into the requirements of the application in order to avoid adding an additional resistor.
Is there a specific interface/application you are looking to protect? I would be very happy to offer our best solutions for your needs!
Best Regards,
Josh Prushing