Part Number: DS90LV804
Hello, I am trying to assess the behavior of contention between sets of LVDS outputs for the subject-line part. To clarify, I mean the following:
- Two separate boards, each with a DS90LV804 installed.
- Each board has a common ground reference.
- One set of OUT pins on one board gets connected to a set of OUT pins on the other board, while powered.
I see the short-circuit rating for this part, however, that is specified to ground, which is not the case here. I'm thinking that contention between two sets of LVDS-driver outputs will not result in more than a 3.5mA draw between one or the other, and obviously the link will not function correctly. However I'd like to confirm for this specific part.
I'll add that this is not a normal operating mode for our design, but it is a possibility if a set of connectors in our system is mis-mated. In our current situation, changing the connector pinout or connector type is not particularly simple, so I'm asking this question to assess the consequences of a mis-mated connector. If it's simply loss of functionality, and no parts stress, we'll probably leave the design as-is as it's easily remedied.
Thank you.