Part Number: TUSB8042
Hi,
I would like to know about TI Tool and at what level of testing it can be used.
We are currently considering testing a USBHUB with TUSB8042 implemented, and we think we can test the communication with TI Tool.
Is it possible to also check the voltage level here?
(If the communication test is OK with this tool, does it maintain the normal range of voltage values specified in the USB 2.0 compliance test?)
Assume that there is an environment where the USB cable is longer and the D+ and D- voltages are less than 300mV.
If we apply the TI tool to this environment, will it pass?
Is there any possibility of restoring the signal and passing the test even if the voltage and timing are slightly off from the specified?
(purpose : I would like to check if the TI tool can also perform voltage tests.)