Part Number: MAX3221
Other Parts Discussed in Thread: TRS3232E
I'm trying to get 2 devices to talk to one. The datasheet sates that "When MAX3221 is unpowered, it can be safely connected to an active remote RS232 device" but it doesn't seem to work when more than one device is connected. I have a main device which is requesting information from two devices. I'm toggling the FORCEOFF until the processor for each device receives the correct ID to enable communication to the main device. RS485 would be more suitable but we are trying to avoid twisted pairs.