Part Number: DP83822H
Other Parts Discussed in Thread: DP83867CR, , DP83869HM, DP83869
Hi,
I have an additional question regarding the answer below in "Related Questions". The Note on P.34 of the DP83867CR Datasheet contains the following information.
----
Q2) If the MAC side is powered off and the PHY is placed in the state of waiting for Magic Packet reception, could you please tell me whether it is necessary to disconnect the MII/GMII/RGMII line using a buffer IC, etc.?
A2) It is not required to disconnect MII/GMII/RGMII lines for WoL application. The pulse is send through GPIO pin instead of MAC interface.
---
It is stated that when using WoL, it is necessary to set BMCR bit[10] Disable = MII Isolate disable.

Is it necessary to set ISOLATE and disconnect the MII/GMII/RGMII line when using WoL? Also, could you please tell me the list of ports that are ISOLATEd with BMCR bit[10]?
Thanks,
Conor