This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF810: Questions of DS250DF810

Part Number: DS250DF810
Other Parts Discussed in Thread: TUSB1104, TDP142, TDP2004, TUSB2044

Dear team,

Do we have suitable solution can replace below? Thanks a lot.

Item

Signal

RVP using model

Description

Vendor

1

USB3.2 Gen 2x2

ANX7434QN

USB 3.2 Gen 2 20G active mux with integrated re-timer and CC Detection

Aanalogix

2

DP

ANX7498QN-AA-R

Aanalogix

3

DP

PTN3816EWY

20 Gbps Per Lane, 4-Lane DisplayPort Linear Redriver

NXP

4

USB3.2 Gen 2x2
DP 1.4

PS8825QFN52GTR-A2

USB-C® 10Gbps Retimer for USB3.2 Gen 2×2 and DP1.4a Alt Mode with Port Controller Supporting TCPCI

Parade

5

DP

PS8483

20Gbps DisplayPortTm Dual Mode Retimer

Parade

Many Thanks,

Jimmy