Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR410: DJ in the output waveform

Part Number: DS160PR410

Hi Team,

I would like to inquire about the concept of DJ (Deterministic Jitter) included in the output waveform of DS160PR410.

According to the datasheet, I noticed that there are multiple DJ values mentioned, namely TDJ-DATA, JITEER_INTRINSIC_SIC_DJ, and JITEER-INTRINSIC-TOTAL. It is stated that this redriver is compatible with PCIeGen4. Upon adding up these DJ values, the maximum value reaches 9.2ps, which is approximately 0.15UI (at 16Gbps).

Does the DJ included in the output waveform of DS160PR410 become the sum of the input waveform's DJ and the aforementioned 9.2ps? And, I thought that if the retimer adds 0.15UI of DJ, it could potentially impose a significant constraint in the link budget. Am I correct in my understanding? From the perspective of DJ, what are the scenarios or situations in which there are benefits to adopting this retimer?