Part Number: DS90UH948-Q1
Other Parts Discussed in Thread: ALP
Hello:
1、UH949 (encoder) and UH948 (deserializer) have the following registers set. Can the screen testpattern be displayed? The power on timing of the screen is already correct (the screen can enter self-test mode)
uh949
{0X03,0Xda},
{0X17,0X9e},
{0X06,0X58},
{0X0d,0X05},
{0X0e,0X03},
{0X54,0X00},
{0X0f,0X05},
{0X07,0X94},
{0X08,0X94},
{0X04,0X90},
{0X04,0X80},
{0X66,0X03},
{0X67,0X0b},
{0X66,0X1a},
{0X67,0X02},
{0X66,0X04},
{0X67,0X84},
{0X66,0X05},
{0X67,0Xc8},
{0X66,0X06},
{0X67,0X53},
{0X66,0X07},
{0X67,0X80},
{0X66,0X08},
{0X67,0X87},
{0X66,0X09},
{0X67,0X43},
{0X66,0X0a},
{0X67,0X28},
{0X66,0X0b},
{0X67,0X02},
{0X66,0X0c},
{0X67,0X28},
{0X66,0X0d},
{0X67,0X08},
{0X65,0X04},
{0X64,0X93},
{0X65,0X04},
{0X64,0X33},
uh948
{0X49,0X60},
{0X1e,0X95},
{0X49,0X62},
{0X1d,0X11},
{0X20,0X11},
{0X21,0X11},
{0X1a,0X01},
{0X02,0X20},
{0X29,0X80},
{0X1e,0X05},
{0X34,0X02},
{0X1d,0X13},
{0X34,0X01},
{0X21,0X99},
{0X20,0X19},
{0X20,0X99},
Specification for TL156VFKS09-00 0828.pdf
TA8301B_V35_R00_V1_sch(2024-02-05).pdf
2、This is the screen parameter,Does the configuration of 0x03 to 0x0c 1a to 0x02 comply with the CLK frequency?

3、The following are the registers configured according to the screen specifications parameters,0x1c reads as 0x3b
uh949
{0X03,0Xda},
{0X17,0X9e},
{0X06,0X58},
{0X0d,0X05},
{0X0e,0X03},
{0X54,0X00},
{0X0f,0X05},
{0X07,0X94},
{0X08,0X94},
{0X04,0X90},
{0X04,0X80},
{0X66,0X03},
{0X67,0X0c},
{0X66,0X1a},
{0X67,0X02},
{0X66,0X04},
{0X67,0Xca},
{0X66,0X05},
{0X67,0Xa7},
{0X66,0X06},
{0X67,0X45},
{0X66,0X07},
{0X67,0X80},
{0X66,0X08},
{0X67,0X87},
{0X66,0X09},
{0X67,0X43},
{0X66,0X0a},
{0X67,0X0f},
{0X66,0X0b},
{0X67,0X02},
{0X66,0X0c},
{0X67,0X0f},
{0X66,0X0d},
{0X67,0X08},
{0X65,0X04},
{0X64,0X93},
{0X65,0X04},
{0X64,0X33},
uh948
{0X49,0X60},
{0X1e,0X95},
{0X49,0X62},
{0X1d,0X11},
{0X20,0X11},
{0X21,0X11},
{0X1a,0X01},
{0X02,0X20},
{0X29,0X80},
{0X1e,0X05},
{0X34,0X02},
{0X1d,0X13},
{0X34,0X01},
{0X21,0X99},
{0X20,0X19},
{0X20,0X99},
There are still some issues with the display screen debugging, and it cannot be disconnected,Please help check,thanks!!!