Other Parts Discussed in Thread: TUSB6250
Hi,
Can someone tell me where to obtain the TUSB6250 firmware source code which is mentioned in the TUSB6250 FAQ? Thanks very much.
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mark,
Please see the attached information.
Do you need more than that?
Regards.
Hi,
Thanks, but as far as I can tell, that file contains just the default binary firmware image, not source code. The TUSB6250 FAQ at http://www.ti.com/litv/pdf/slla171a says (on page 9):
"Texas Instruments provides a clickwrapped version of the source code that
includes a document that describes the projects settings, version numbering
system , precompiler build options and directory structure. Compiling the source
code can be accomplished with different compilers: Kiel, IAR, Tasking. The
supplied source code was build and compiled using a Tasking compiler and there is
some effort involved with porting the code to another compiler."
So it seems the source is available, but I couldn't find it on the TI web site.
Mark
Mark,
In order to receive the firmware source code, you will need to send your request to usb@ti.com.
We cannot post the source code on ti.com due to potential export control requirements.