Part Number: TUSB522P
Hi,
I purchased TUSB522P EVM. It works fine with USB port on a laptop. would like to test our USB3.0 cable with BERT Scope BSA286CL. I can't get the output through the EVM. Below is the block diagram I have for the test. the input signal is 500mv Vp-p, 5Gbps. 5V power is provided to the EVM from an external power supply. questions:
1. is this test setup correct?
2. it doesn't handshaking process to work does it?
3. looking for your recommendation and suggestions.
thanks
bin