Part Number: TUSB8041
Other Parts Discussed in Thread: TUSB4020BI, , TUSB8020B
Hi
I'm designing a USB HUB product.
My product requirements are following.
- USB3.2 upstream port x1
- USB3.2 downstream port x4
- a USB2.0 device in the product
I plan to use TUSB8041 but it doesn't have enough downstream ports for my requirements.
Therefore, I'm planning to use two HUBs in a cascade connection within the product.
Question : Is it possible to use TUSB8041 and TUSB4020BI as shown in "Block Diagram A" in the attached file?
I know I can achieve what I want by using two TUSB8041 as shown in "Block Diagram B", but I'd like to keep the cost as low as possible.
So I'd like to apply "Block Diagram A".
If you have any other good ideas, would you let me know?