Part Number: DS90UB638-Q1
Other Parts Discussed in Thread: DS90UB635-Q1,
I have a DS90UB638-Q1 / DS90UB635-Q1 system running.
I would like to test at a lower forward frequency.
Table 7-8 (Clocking Modes) of the 635 data sheet describes a Synchronous (Half-rate) mode. I would like to test that mode.
I understand the first step is to configure the BC_FREQ_SELECT field in register 0x58 of the 638 device.
On power up, register 0x58 reads 0x1E, indicating a 50Mbps back channel was configured by the MODE Pin strapping. This is expected.
I try to write 0x1D to change the mode to 25 Mbps back channel.
Register 0x58 always reads back 0x1E.
Am I missing some step in this configuration?