Part Number: DS90UB947-Q1
Hello,
I am using the EVM DS90UB947 encoder board as a pattern generator, and it is working well with the '946 and '948 decoder boards.
I will be creating a new Printed Circuit Board as part pf a text fixture, board space is tight.
When the DS90UB947 is working as a pattern Generator with internal Clocks;
Do I need to install 100 ohm termination resistors on the CLK+/` and D0~D7 +/- input lines ?
or can I leave them floating?
Thanks,
James