This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1039-Q1: Tlin recommend

Part Number: TLIN1039-Q1

Hello,

Our customer is looking for such a TLIN. Could you please recommend the device.

The material type:
L IN transceiver with local and remote wake-up
The material description:
LIN
IC_10 21_40 125°C.
Compatible
LIN standard LIN 2.x.
, SAE J2602 ISO 17987 4
Maximum LIN speed 20 kbps
VLIN ≥ ±40 V.
VBAT supply Voltage ≥ 4.5 40V, Max. Withstand pressure 0.3 ~+ 40 V.
IBAT supply current ≤ 22 uA
Sleep mode V LIN = V WAKE_N V BAT; V TXD = 0 V; V SLP_n = 0 V.
VCC supply voltage ≥ 4.5~5.5V,
Max. Withstand pressure 0.3 ~+ 6V
VTXD high threshold minimum ≥ 2 V,
Low threshold ≤ 0.8V max.,
Max. Withstand pressure 0.3 ~+ 6V
VESD ≥ ±6 kV IEC 61000 4 2 at pins LIN, W AKE_N, V BAT
AEC Q100

Thanks,

Yuhao