Part Number: DP83TC813S-Q1
Hello
We are trying to enable the PMA compliance test mode 1 by checking on the BMSR register and confirm that the link is Up then write 0x2000 to register 0x1836 through the indirect accesses.
And we need to know what is the expected output waveform and on which pins ? to make sure that the configuration is reflected correctly into the registers and the mode is functional.
shall we monitor the differential output pins H and L and expect to have a square wave like the screenshoot below repeated continuously without any gaps in between?

As what we are currently obtaining when monitoring the differential output High pin is that the product always enters/exits test mode the time during which the product is in test mode is consistent to 800µs but the time between two test modes is variable (always few tens or hundreds of ms).
Screenshot attached for your reference, Ethernet is on channel 3 in blue and in the picture the product is in test mode for 800µs separated by 20ms around the two cursors X1 and X2.

When I zoom in again:

Appreciate your prompt response.