Part Number: P82B96
I am wondering if it is possible to use two P82B96D (one Master side and one Slave side) with two different VCC voltages: for example the Master side powered with a 12V VCC to wich the bus pull-up resistor are tied, while the Slave side is powered with a VCC of 5V. On the data sheet I did not find anything preventing or mentioning this specific configuration. Except on a paragraph related to Tx and Ty where it is explicitally stated that voltages on this pins can exceed the VCC voltage because they are not provided with the ESD diodes protection to VCC/GND. If the same happens to Rx and Ry (not mentioned in the data sheet) I believe this configuration could work.
Any feedback?
Reagards.
Maurizio