Part Number: SN65HVD73
Other Parts Discussed in Thread: SN65HVD70
Hello,
we are using the SN65HVD73 transceiver with an UART input. The baudrate of the UART port is quite low (115200) and the cable length also short (<5m), so i thought we won't need any complex noise filtering or multiple termination resistors. Can we use this circuit? Is the termination res value of R62/R133 appropriate, or should it be adjusted? Do we need to add any additional filtering like chokes, or any other elements?
Thanks in advance!