Part Number: DS250DF410
Hi Team,
If would like to use DS250DF410 support 1.25Gbps data rate, is follow the step as below E2E thread show can also achieve it? Since it looks like only change to bypass mode.
And my second question is why need to set data rate as 10G or 25G? Will 10G or 25G data rate setting affect bypass mode performance in 1G data rate actually?
My third question is that if in CDR bypass mode then I still can set to mode2 or 3? (the EQ setting and DFE will auto adaptive at power on) Or just can use manual mode setting EQ/Gain/DFE parameter?
Thanks.
Best Regards,
Roy