Part Number: DP83822IF
hi.
Strap set up for DP83822IF fiber drive
After testing, the pull-down straps of RX_D0 and RX_D1 did not work properly
If the pull-down strap of RX_D0, RX_D1 is applied with RH 2.49K pull-up resistance, it is set datasheet mode 4
If you check the actual register Set to Mode_1
Is the data sheet wrong?
Datasheet does not say to use pull-up 2.49k for RX_D0 and RX_D1 when using Fiber mode
Please check with the company

<- Pull-down MODE Open : mode 2 set
<- Pull-down MODE 4 set : mode 1 set