Hi,
DS250DF230 check the HEO and VEO when it tries to lock to the input.
If the HEO or VEO decreases bellow than the LOKC threshold, does it de-assert lock or keep lock despite of poor HEO or VEO?
Best Regards,
Nishie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
DS250DF230 check the HEO and VEO when it tries to lock to the input.
If the HEO or VEO decreases bellow than the LOKC threshold, does it de-assert lock or keep lock despite of poor HEO or VEO?
Best Regards,
Nishie
Hi Nishie-san,
Lock is de-asserted if HEO/VEO decrease below the threshold.
There are a couple registers impacting this. Please see data sheet for more details.
| Register | Field Name | Description |
| 0x67[5] | HV_LOCKMON_EN | Controls periodic monitoring of HEO/VEO for LOCK qualification. |
| 0x76[7:4] | POST_LOCK_VEO_THR[3:0] | VEO threshold after LOCK is established. |
| 0x76[3:0] | POST_LOCK_HEO_THR[3:0] | HEO threshold after LOCK is established. |
Thanks,
Drew
Hi Drew-san,
Thank you for your support.
Are you sure lock is de-asserted if HEO/VEO decrease below the threshold? Could you check it again?
The reason is that the lock does not come off even though the customer's device has a lower limit of HEO.
Programmable Guide also has the following options:
------------------------------------
7.15 HEO/VEO Lock Monitoring
Enable or disable Horizontal Eye Opening (HEO) and Vertical Eye Opening (VEO) monitoring for CDR lock
qualification. HEO/VEO lock monitoring will cause the CDR to fall out of lock if the HEO or VEO fall below the
configured threshold.
------------------------------------
Therefore, please check if Lock is not released.
Best Regards,
Nishie
Hi Nishie-san,
How has the customer configured register 0x76? What HEO is the customer observing where they expect lock to drop?
Thanks,
Drew
Hi Drew-san,
How has the customer configured register 0x76?
Register 0x76 is set to 0x21.
What HEO is the customer observing where they expect lock to drop?
I will check.
The 5th bit of register 0x67 says "1: Enable periodic monitoring of HEO/VEO for lock qualification". What is the period of "periodic monitoring"? Please let me know if you have any information such as monitoring every X ms.

Best Regards,
Nishie
Hi Nishie-san,
I'll look into this and get back to you early next week.
Thanks,
Drew
Hi Nishie-san,
I've discussed with my colleagues, but we don't have documentation readily available on exactly what the period of the periodic monitoring is. I can say that EOM is not constantly running due to power consumption.
Does the customer suspect an issue with their application due to HEO/VEO lock check period?
Thanks,
Drew
Hi Drew-san,
Thank you for confirming. Let the customer know that we do not have accurate information about the monitoring period.
As shown in the following thread, a LOCK with an unintended data rate has occurred. To avoid this, we are considering countermeasures by changing the threshold of HEO/VEO.
Best Regards,
Nishie