Part Number: DS250DF230
Hi,
DS250DF230 check the HEO and VEO when it tries to lock to the input.
If the HEO or VEO decreases bellow than the LOKC threshold, does it de-assert lock or keep lock despite of poor HEO or VEO?
Best Regards,
Nishie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF230
Hi,
DS250DF230 check the HEO and VEO when it tries to lock to the input.
If the HEO or VEO decreases bellow than the LOKC threshold, does it de-assert lock or keep lock despite of poor HEO or VEO?
Best Regards,
Nishie
Hi Nishie-san,
Lock is de-asserted if HEO/VEO decrease below the threshold.
There are a couple registers impacting this. Please see data sheet for more details.
| Register | Field Name | Description |
| 0x67[5] | HV_LOCKMON_EN | Controls periodic monitoring of HEO/VEO for LOCK qualification. |
| 0x76[7:4] | POST_LOCK_VEO_THR[3:0] | VEO threshold after LOCK is established. |
| 0x76[3:0] | POST_LOCK_HEO_THR[3:0] | HEO threshold after LOCK is established. |
Thanks,
Drew
Hi Drew-san,
Thank you for your support.
Are you sure lock is de-asserted if HEO/VEO decrease below the threshold? Could you check it again?
The reason is that the lock does not come off even though the customer's device has a lower limit of HEO.
Programmable Guide also has the following options:
------------------------------------
7.15 HEO/VEO Lock Monitoring
Enable or disable Horizontal Eye Opening (HEO) and Vertical Eye Opening (VEO) monitoring for CDR lock
qualification. HEO/VEO lock monitoring will cause the CDR to fall out of lock if the HEO or VEO fall below the
configured threshold.
------------------------------------
Therefore, please check if Lock is not released.
Best Regards,
Nishie
Hi Nishie-san,
How has the customer configured register 0x76? What HEO is the customer observing where they expect lock to drop?
Thanks,
Drew
Hi Drew-san,
How has the customer configured register 0x76?
Register 0x76 is set to 0x21.
What HEO is the customer observing where they expect lock to drop?
I will check.
The 5th bit of register 0x67 says "1: Enable periodic monitoring of HEO/VEO for lock qualification". What is the period of "periodic monitoring"? Please let me know if you have any information such as monitoring every X ms.

Best Regards,
Nishie
Hi Nishie-san,
I'll look into this and get back to you early next week.
Thanks,
Drew
Hi Nishie-san,
I've discussed with my colleagues, but we don't have documentation readily available on exactly what the period of the periodic monitoring is. I can say that EOM is not constantly running due to power consumption.
Does the customer suspect an issue with their application due to HEO/VEO lock check period?
Thanks,
Drew
Hi Drew-san,
Thank you for confirming. Let the customer know that we do not have accurate information about the monitoring period.
As shown in the following thread, a LOCK with an unintended data rate has occurred. To avoid this, we are considering countermeasures by changing the threshold of HEO/VEO.
Best Regards,
Nishie