Part Number: DP83867IR
I have DP83867 PHY on GEM1 MDIO interface on a custom board.
The driver is up and PHY is detected & can be seen from u-boot. And also able to ping Link partner as well.
But I am not able to ping the LP in Linux, can only ping myself.
Here is my u-boot log of PHY detection and PHY dump :
Xilinx Zynq MP First Stage Boot Loader
Release 2022.2 Oct 7 2022 - 04:56:16
NOTICE: BL31: v2.6(release):xlnx_rebase_v2.6_2022.1_update3-18-g0897efd45
NOTICE: BL31: Built : 03:55:03, Sep 9 2022
U-Boot 2022.01 (Sep 20 2022 - 06:35:33 +0000)
CPU: ZynqMP
Silicon: v3
Board: Xilinx ZynqMP
DRAM: 2 GiB
PMUFW: v1.1
PMUFW no permission to change config object
EL Level: EL2
Chip ID: zu4
NAND: 0 MiB
MMC: mmc@ff160000: 0
Loading Environment from FAT... *** Warning - some problems detected reading environment; recovered successfully
OK
In: serial
Out: serial
Err: serial
Net: PHY reset timed out
ZYNQ GEM: ff0c0000, mdio bus ff0c0000, phyaddr 0, interface rgmii-id
Warning: ethernet@ff0c0000 MAC addresses don't match:
Address in DT is 00:01:02:03:04:05
Address in environment is 70:b3:d5:9a:60:95
eth0: ethernet@ff0c0000
scanning bus for devices...
starting USB...
Bus usb@fe200000: Register 2000440 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@fe200000 for devices... 2 USB Device(s) found
scanning usb for storage devices... 1 Storage Device(s) found
Hit any key to stop autoboot: 0
ZynqMP>
ZynqMP>
ZynqMP>
ZynqMP> mii info
PHY 0x05: OUI = 0x80028, Model = 0x23, Rev = 0x01, 1000baseT, FDX
ZynqMP> mdio list
eth0:
0 - TI DP83867 <--> ethernet@ff0c0000
ZynqMP>
ZynqMP> mii read 0x5 0-9
addr=05 reg=00 data=1140
addr=05 reg=01 data=7969
addr=05 reg=02 data=2000
addr=05 reg=03 data=A231
addr=05 reg=04 data=01E1
addr=05 reg=05 data=C1E1
addr=05 reg=06 data=007F
addr=05 reg=07 data=2001
addr=05 reg=08 data=6801
addr=05 reg=09 data=0300
ZynqMP>
Here is my device-tree :
&gem1 {
phy-handle = <&phy1>;
local-mac-address = [00 01 02 03 04 05];
xlnx,ptp-enet-clock = <0x0>;
phy-mode = "rgmii-id";
status = "okay";
//clock-frequency = <2500000>;
mdio {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
phy1:phy@0{
status = "okay";
device_type = "ethernet-phy";
compatible = "ethernet-phy-id2000.a231", "ethernet-phy-ieee802.3-c22";
reg = <0>;
ti,rx-internal-delay = <0x8>;
ti,tx-internal-delay = <0x0>;
ti,fifo-depth = <0x1>;
};
};
};
Here is the complete boot-up logs :
Xilinx Zynq MP First Stage Boot Loader
Release 2022.2 Oct 7 2022 - 04:56:16
NOTICE: BL31: v2.6(release):xlnx_rebase_v2.6_2022.1_update3-18-g0897efd45
NOTICE: BL31: Built : 03:55:03, Sep 9 2022
U-Boot 2022.01 (Sep 20 2022 - 06:35:33 +0000)
CPU: ZynqMP
Silicon: v3
Board: Xilinx ZynqMP
DRAM: 2 GiB
PMUFW: v1.1
PMUFW no permission to change config object
EL Level: EL2
Chip ID: zu4
NAND: 0 MiB
MMC: mmc@ff160000: 0
Loading Environment from FAT... *** Warning - some problems detected reading environment; recovered successfully
OK
In: serial
Out: serial
Err: serial
Net: PHY reset timed out
ZYNQ GEM: ff0c0000, mdio bus ff0c0000, phyaddr 0, interface rgmii-id
Warning: ethernet@ff0c0000 MAC addresses don't match:
Address in DT is 00:01:02:03:04:05
Address in environment is 70:b3:d5:9a:60:95
eth0: ethernet@ff0c0000
scanning bus for devices...
starting USB...
Bus usb@fe200000: Register 2000440 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb@fe200000 for devices... 2 USB Device(s) found
scanning usb for storage devices... 1 Storage Device(s) found
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1...
Found U-Boot script /boot.scr
2777 bytes read in 15 ms (180.7 KiB/s)
## Executing script at 20000000
Trying to load boot images from mmc0
56783488 bytes read in 4059 ms (13.3 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
Using 'conf-system-top.dtb' configuration
Trying 'kernel-1' kernel subimage
Description: Linux kernel
Created: 2022-10-03 7:50:07 UTC
Type: Kernel Image
Compression: gzip compressed
Data Start: 0x100000fc
Data Size: 9367099 Bytes = 8.9 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x00200000
Entry Point: 0x00200000
Hash algo: sha256
Hash value: f83ee5af3d2342a6fa3e0f077ad78ba7170c18e446a9ff3db6e5ace9917507cc
Verifying Hash Integrity ... sha256+ OK
## Loading ramdisk from FIT Image at 10000000 ...
Using 'conf-system-top.dtb' configuration
Trying 'ramdisk-1' ramdisk subimage
Description: petalinux-image-minimal
Created: 2022-10-03 7:50:07 UTC
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0x108fa460
Data Size: 47368360 Bytes = 45.2 MiB
Architecture: AArch64
OS: Linux
Load Address: unavailable
Entry Point: unavailable
Hash algo: sha256
Hash value: 38777a1d7442e50f3717fff3b87c6b1c7e7fac59100037bd9d940abe66fe29e6
Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at 10000000 ...
Using 'conf-system-top.dtb' configuration
Trying 'fdt-system-top.dtb' fdt subimage
Description: Flattened Device Tree blob
Created: 2022-10-03 7:50:07 UTC
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0x108ef048
Data Size: 45895 Bytes = 44.8 KiB
Architecture: AArch64
Hash algo: sha256
Hash value: 0c64bb67f644637e2f57e7c3ab3f9a16617e525abb0614e8ea9a65a3e7a591f6
Verifying Hash Integrity ... sha256+ OK
Booting using the fdt blob at 0x108ef048
Uncompressing Kernel Image
Loading Ramdisk to 78ecc000, end 7bbf88a8 ... OK
Loading Device Tree to 0000000078ebd000, end 0000000078ecb346 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.15.36-xilinx-v2022.2 (oe-user@oe-host) (aarch64-xilinx-linux-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.37.20210721) #1 SMP Mon Oct 3 07:50:07 UTC 2022
[ 0.000000] Machine model: xlnx,zynqmp
[ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[ 0.000000] printk: bootconsole [cdns0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000000000000-0x000000007fefffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000000000000-0x000000007fefffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000007fefffff]
[ 0.000000] On node 0, zone DMA32: 256 pages in unavailable ranges
[ 0.000000] cma: Reserved 256 MiB at 0x0000000068c00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 18 pages/cpu s34776 r8192 d30760 u73728
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 515844
[ 0.000000] Kernel command line: earlycon console=ttyPS0,115200 clk_ignore_unused root=/dev/ram0 rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1725284K/2096128K available (14080K kernel code, 994K rwdata, 3964K rodata, 2176K init, 573K bss, 108700K reserved, 262144K cma-reserved)
[ 0.000000] rcu: Hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=16 to nr_cpu_ids=4.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] random: get_random_bytes called from start_kernel+0x474/0x6d8 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b0074340, max_idle_ns: 440795202884 ns
[ 0.000000] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255543ns
[ 0.008315] Console: colour dummy device 80x25
[ 0.012393] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133332)
[ 0.022666] pid_max: default: 32768 minimum: 301
[ 0.027455] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.034609] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.043415] rcu: Hierarchical SRCU implementation.
[ 0.047386] EFI services will not be available.
[ 0.051784] smp: Bringing up secondary CPUs ...
[ 0.056508] Detected VIPT I-cache on CPU1
[ 0.056544] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.056934] Detected VIPT I-cache on CPU2
[ 0.056957] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.057325] Detected VIPT I-cache on CPU3
[ 0.057348] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.057392] smp: Brought up 1 node, 4 CPUs
[ 0.091607] SMP: Total of 4 processors activated.
[ 0.096279] CPU features: detected: 32-bit EL0 Support
[ 0.101382] CPU features: detected: CRC32 instructions
[ 0.106522] CPU: All CPU(s) started at EL2
[ 0.110564] alternatives: patching kernel code
[ 0.115886] devtmpfs: initialized
[ 0.123007] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.127953] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.140485] pinctrl core: initialized pinctrl subsystem
[ 0.140958] DMI not present or invalid.
[ 0.144120] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.150795] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.156889] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.164683] audit: initializing netlink subsys (disabled)
[ 0.170079] audit: type=2000 audit(0.108:1): state=initialized audit_enabled=0 res=1
[ 0.170425] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.184502] ASID allocator initialised with 65536 entries
[ 0.189921] Serial: AMBA PL011 UART driver
[ 0.211483] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.212542] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.219213] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.225875] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 1.301747] cryptd: max_cpu_qlen set to 1000
[ 1.325517] DRBG: Continuing without Jitter RNG
[ 1.429336] raid6: neonx8 gen() 2133 MB/s
[ 1.497383] raid6: neonx8 xor() 1581 MB/s
[ 1.565454] raid6: neonx4 gen() 2180 MB/s
[ 1.633506] raid6: neonx4 xor() 1555 MB/s
[ 1.701571] raid6: neonx2 gen() 2066 MB/s
[ 1.769625] raid6: neonx2 xor() 1430 MB/s
[ 1.837696] raid6: neonx1 gen() 1763 MB/s
[ 1.905753] raid6: neonx1 xor() 1212 MB/s
[ 1.973811] raid6: int64x8 gen() 1363 MB/s
[ 2.041874] raid6: int64x8 xor() 773 MB/s
[ 2.109949] raid6: int64x4 gen() 1599 MB/s
[ 2.177998] raid6: int64x4 xor() 850 MB/s
[ 2.246075] raid6: int64x2 gen() 1397 MB/s
[ 2.314126] raid6: int64x2 xor() 750 MB/s
[ 2.382206] raid6: int64x1 gen() 1031 MB/s
[ 2.450242] raid6: int64x1 xor() 517 MB/s
[ 2.450281] raid6: using algorithm neonx4 gen() 2180 MB/s
[ 2.454235] raid6: .... xor() 1555 MB/s, rmw enabled
[ 2.459170] raid6: using neon recovery algorithm
[ 2.464299] iommu: Default domain type: Translated
[ 2.468604] iommu: DMA domain TLB invalidation policy: strict mode
[ 2.475035] SCSI subsystem initialized
[ 2.478693] usbcore: registered new interface driver usbfs
[ 2.484031] usbcore: registered new interface driver hub
[ 2.489293] usbcore: registered new device driver usb
[ 2.494354] mc: Linux media interface: v0.10
[ 2.498547] videodev: Linux video capture interface: v2.00
[ 2.504010] pps_core: LinuxPPS API ver. 1 registered
[ 2.508909] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 2.517999] PTP clock support registered
[ 2.521903] EDAC MC: Ver: 3.0.0
[ 2.525262] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels.
[ 2.533669] FPGA manager framework
[ 2.536965] Advanced Linux Sound Architecture Driver Initialized.
[ 2.543209] Bluetooth: Core ver 2.22
[ 2.546462] NET: Registered PF_BLUETOOTH protocol family
[ 2.551728] Bluetooth: HCI device and connection manager initialized
[ 2.558045] Bluetooth: HCI socket layer initialized
[ 2.562887] Bluetooth: L2CAP socket layer initialized
[ 2.567909] Bluetooth: SCO socket layer initialized
[ 2.573050] clocksource: Switched to clocksource arch_sys_counter
[ 2.578933] VFS: Disk quotas dquot_6.6.0
[ 2.582734] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 2.593786] NET: Registered PF_INET protocol family
[ 2.594452] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 2.602630] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 2.610226] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 2.618176] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 2.625528] TCP: Hash tables configured (established 16384 bind 16384)
[ 2.631887] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 2.638526] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 2.645679] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 2.651478] RPC: Registered named UNIX socket transport module.
[ 2.657094] RPC: Registered udp transport module.
[ 2.661760] RPC: Registered tcp transport module.
[ 2.666427] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 2.672833] PCI: CLS 0 bytes, default 64
[ 2.676855] Trying to unpack rootfs image as initramfs...
[ 2.682763] armv8-pmu pmu: hw perfevents: no interrupt-affinity property, guessing.
[ 2.689970] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 4.933387] Freeing initrd memory: 46256K
[ 4.989935] Initialise system trusted keyrings
[ 4.990069] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[ 4.995863] NFS: Registering the id_resolver key type
[ 5.000182] Key type id_resolver registered
[ 5.004364] Key type id_legacy registered
[ 5.008315] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 5.014961] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 5.022324] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 5.066657] NET: Registered PF_ALG protocol family
[ 5.066703] xor: measuring software checksum speed
[ 5.074734] 8regs : 2363 MB/sec
[ 5.078400] 32regs : 2799 MB/sec
[ 5.083477] arm64_neon : 2307 MB/sec
[ 5.083533] xor: using function: 32regs (2799 MB/sec)
[ 5.088556] Key type asymmetric registered
[ 5.092620] Asymmetric key parser 'x509' registered
[ 5.097498] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 5.104819] io scheduler mq-deadline registered
[ 5.109315] io scheduler kyber registered
[ 5.141267] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 5.143074] Serial: AMBA driver
[ 5.145982] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 5.155349] brd: module loaded
[ 5.158785] loop: module loaded
[ 5.159720] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 5.166575] tun: Universal TUN/TAP device driver, 1.6
[ 5.168792] CAN device driver interface
[ 5.173343] usbcore: registered new interface driver asix
[ 5.177921] usbcore: registered new interface driver ax88179_178a
[ 5.183959] usbcore: registered new interface driver cdc_ether
[ 5.189754] usbcore: registered new interface driver net1080
[ 5.195376] usbcore: registered new interface driver cdc_subset
[ 5.201258] usbcore: registered new interface driver zaurus
[ 5.206805] usbcore: registered new interface driver cdc_ncm
[ 5.213439] usbcore: registered new interface driver uas
[ 5.217705] usbcore: registered new interface driver usb-storage
[ 5.224240] rtc_zynqmp ffa60000.rtc: registered as rtc0
[ 5.228847] rtc_zynqmp ffa60000.rtc: setting system clock to 1987-01-05T19:13:57 UTC (536872437)
[ 5.237627] i2c_dev: i2c /dev entries driver
[ 5.243693] usbcore: registered new interface driver uvcvideo
[ 5.247970] Bluetooth: HCI UART driver ver 2.3
[ 5.251932] Bluetooth: HCI UART protocol H4 registered
[ 5.257035] Bluetooth: HCI UART protocol BCSP registered
[ 5.262327] Bluetooth: HCI UART protocol LL registered
[ 5.267414] Bluetooth: HCI UART protocol ATH3K registered
[ 5.272788] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 5.279039] Bluetooth: HCI UART protocol Intel registered
[ 5.284381] Bluetooth: HCI UART protocol QCA registered
[ 5.289583] usbcore: registered new interface driver bcm203x
[ 5.295215] usbcore: registered new interface driver bpa10x
[ 5.300738] usbcore: registered new interface driver bfusb
[ 5.306190] usbcore: registered new interface driver btusb
[ 5.311651] usbcore: registered new interface driver ath3k
[ 5.317143] EDAC MC: ECC not enabled
[ 5.320735] EDAC DEVICE0: Giving out device to module edac controller cache_err: DEV edac (POLLED)
[ 5.329681] EDAC DEVICE1: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[ 5.342083] sdhci: Secure Digital Host Controller Interface driver
[ 5.347779] sdhci: Copyright(c) Pierre Ossman
[ 5.352099] sdhci-pltfm: SDHCI platform and OF driver helper
[ 5.358064] ledtrig-cpu: registered to indicate activity on CPUs
[ 5.363790] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 5.370164] zynqmp_firmware_probe Platform Management API v1.1
[ 5.375889] zynqmp_firmware_probe Trustzone version v1.0
[ 5.408509] securefw securefw: securefw probed
[ 5.408645] zynqmp_aes firmware:zynqmp-firmware:zynqmp-aes: The zynqmp-aes driver shall be deprecated in 2022.2 and removed in 2023.1
[ 5.419477] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
[ 5.424903] zynqmp_aes firmware:zynqmp-firmware:zynqmp-aes: AES Successfully Registered
[ 5.432954] zynqmp-keccak-384 firmware:zynqmp-firmware:sha384: The zynqmp-sha-deprecated driver shall be deprecated in 2022.2 and removed in 2023.1 release
[ 5.446745] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
[ 5.453011] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[ 5.458504] usbcore: registered new interface driver usbhid
[ 5.463895] usbhid: USB HID core driver
[ 5.470790] ARM CCI_400_r1 PMU driver probed
[ 5.471444] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[ 5.478769] usbcore: registered new interface driver snd-usb-audio
[ 5.485328] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 5.492739] Initializing XFRM netlink socket
[ 5.496330] NET: Registered PF_INET6 protocol family
[ 5.501610] Segment Routing with IPv6
[ 5.504814] In-situ OAM (IOAM) with IPv6
[ 5.508768] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 5.514901] NET: Registered PF_PACKET protocol family
[ 5.519610] NET: Registered PF_KEY protocol family
[ 5.524371] can: controller area network core
[ 5.528708] NET: Registered PF_CAN protocol family
[ 5.533441] can: raw protocol
[ 5.536376] can: broadcast manager protocol
[ 5.540536] can: netlink gateway - max_hops=1
[ 5.544928] Bluetooth: RFCOMM TTY layer initialized
[ 5.549710] Bluetooth: RFCOMM socket layer initialized
[ 5.554814] Bluetooth: RFCOMM ver 1.11
[ 5.558527] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 5.563800] Bluetooth: BNEP filters: protocol multicast
[ 5.568991] Bluetooth: BNEP socket layer initialized
[ 5.573919] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 5.579805] Bluetooth: HIDP socket layer initialized
[ 5.584759] 8021q: 802.1Q VLAN Support v1.8
[ 5.588984] 9pnet: Installing 9P2000 support
[ 5.593145] Key type dns_resolver registered
[ 5.597469] registered taskstats version 1
[ 5.601431] Loading compiled-in X.509 certificates
[ 5.607263] Btrfs loaded, crc32c=crc32c-generic, zoned=no, fsverity=no
[ 5.621131] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 49, base_baud = 6249999) is a xuartps
[ 5.630158] printk: console [ttyPS0] enabled
[ 5.630158] printk: console [ttyPS0] enabled
[ 5.634452] printk: bootconsole [cdns0] disabled
[ 5.634452] printk: bootconsole [cdns0] disabled
[ 5.643765] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 50, base_baud = 6249999) is a xuartps
[ 5.658768] of-fpga-region fpga-full: FPGA Region probed
[ 5.664237] gpiochip_find_base: cannot find free range
[ 5.669369] gpiochip_add_data_with_key: GPIOs 0..173 (zynqmp_gpio) failed to register, -28
[ 5.677635] zynq-gpio ff0a0000.gpio: Failed to add gpio chip
[ 5.683334] zynq-gpio: probe of ff0a0000.gpio failed with error -28
[ 5.690232] random: fast init done
[ 5.706044] random: crng init done
[ 5.791240] irq 53: nobody cared (try booting with the "irqpoll" option)
[ 5.797931] CPU: 0 PID: 8 Comm: kworker/u8:0 Not tainted 5.15.36-xilinx-v2022.2 #1
[ 5.805489] Hardware name: xlnx,zynqmp (DT)
[ 5.809657] Workqueue: events_unbound deferred_probe_work_func
[ 5.815489] Call trace:
[ 5.817919] dump_backtrace+0x0/0x190
[ 5.821574] show_stack+0x18/0x30
[ 5.824881] dump_stack_lvl+0x7c/0xa0
[ 5.828535] dump_stack+0x18/0x34
[ 5.831842] __report_bad_irq+0x4c/0x138
[ 5.835757] note_interrupt+0x2f8/0x35c
[ 5.839584] handle_irq_event+0xec/0x120
[ 5.843499] handle_fasteoi_irq+0xc0/0x220
[ 5.847587] handle_domain_irq+0x60/0x90
[ 5.851502] gic_handle_irq+0x74/0xa0
[ 5.855157] do_interrupt_handler+0x34/0x60
[ 5.859332] el1_interrupt+0x30/0x50
[ 5.862899] el1h_64_irq_handler+0x18/0x24
[ 5.866987] el1h_64_irq+0x78/0x7c
[ 5.870381] _stext+0xa8/0x2a4
[ 5.873428] irq_exit+0xbc/0x100
[ 5.876649] handle_domain_irq+0x64/0x90
[ 5.880563] gic_handle_irq+0x74/0xa0
[ 5.884218] call_on_irq_stack+0x2c/0x60
[ 5.888132] do_interrupt_handler+0x54/0x60
[ 5.892307] el1_interrupt+0x30/0x50
[ 5.895875] el1h_64_irq_handler+0x18/0x24
[ 5.899963] el1h_64_irq+0x78/0x7c
[ 5.903357] __setup_irq+0x4bc/0x7b0
[ 5.906925] request_threaded_irq+0xe8/0x1b0
[ 5.911186] xilinx_dma_probe+0x4c0/0xc50
[ 5.915188] platform_probe+0x68/0xe0
[ 5.918842] really_probe.part.0+0x9c/0x30c
[ 5.923017] __driver_probe_device+0x98/0x144
[ 5.927366] driver_probe_device+0x44/0x11c
[ 5.931541] __device_attach_driver+0xb4/0x120
[ 5.935977] bus_for_each_drv+0x78/0xd0
[ 5.939805] __device_attach+0xdc/0x184
[ 5.943633] device_initial_probe+0x14/0x20
[ 5.947808] bus_probe_device+0x9c/0xa4
[ 5.951636] deferred_probe_work_func+0x88/0xc0
[ 5.956158] process_one_work+0x1d8/0x390
[ 5.960159] worker_thread+0x298/0x4e0
[ 5.963901] kthread+0x120/0x130
[ 5.967121] ret_from_fork+0x10/0x20
[ 5.970689] handlers:
[ 5.972945] [<00000000f33a20fd>] xilinx_dma_irq_handler
[ 5.978162] Disabling IRQ #53
[ 6.079984] irq 54: nobody cared (try booting with the "irqpoll" option)
[ 6.086672] CPU: 0 PID: 8 Comm: kworker/u8:0 Not tainted 5.15.36-xilinx-v2022.2 #1
[ 6.094232] Hardware name: xlnx,zynqmp (DT)
[ 6.098399] Workqueue: events_unbound deferred_probe_work_func
[ 6.104223] Call trace:
[ 6.106653] dump_backtrace+0x0/0x190
[ 6.110308] show_stack+0x18/0x30
[ 6.113615] dump_stack_lvl+0x7c/0xa0
[ 6.117269] dump_stack+0x18/0x34
[ 6.120576] __report_bad_irq+0x4c/0x138
[ 6.124491] note_interrupt+0x2f8/0x35c
[ 6.128319] handle_irq_event+0xec/0x120
[ 6.132234] handle_fasteoi_irq+0xc0/0x220
[ 6.136322] handle_domain_irq+0x60/0x90
[ 6.140237] gic_handle_irq+0x74/0xa0
[ 6.143891] call_on_irq_stack+0x2c/0x60
[ 6.147806] do_interrupt_handler+0x54/0x60
[ 6.151981] el1_interrupt+0x30/0x50
[ 6.155548] el1h_64_irq_handler+0x18/0x24
[ 6.159637] el1h_64_irq+0x78/0x7c
[ 6.163031] __setup_irq+0x4bc/0x7b0
[ 6.166598] request_threaded_irq+0xe8/0x1b0
[ 6.170860] xilinx_dma_probe+0x4c0/0xc50
[ 6.174862] platform_probe+0x68/0xe0
[ 6.178516] really_probe.part.0+0x9c/0x30c
[ 6.182691] __driver_probe_device+0x98/0x144
[ 6.187040] driver_probe_device+0x44/0x11c
[ 6.191215] __device_attach_driver+0xb4/0x120
[ 6.195650] bus_for_each_drv+0x78/0xd0
[ 6.199478] __device_attach+0xdc/0x184
[ 6.203306] device_initial_probe+0x14/0x20
[ 6.207481] bus_probe_device+0x9c/0xa4
[ 6.211309] deferred_probe_work_func+0x88/0xc0
[ 6.215831] process_one_work+0x1d8/0x390
[ 6.219833] worker_thread+0x298/0x4e0
[ 6.223574] kthread+0x120/0x130
[ 6.226794] ret_from_fork+0x10/0x20
[ 6.230362] handlers:
[ 6.232619] [<00000000f33a20fd>] xilinx_dma_irq_handler
[ 6.237835] Disabling IRQ #54
[ 6.240914] xilinx-vdma a0080000.dma: Xilinx AXI DMA Engine Driver Probed!!
[ 6.248161] xilinx-zynqmp-dma fd500000.dma-controller: ZynqMP DMA driver Probe success
[ 6.256254] xilinx-zynqmp-dma fd510000.dma-controller: ZynqMP DMA driver Probe success
[ 6.264340] xilinx-zynqmp-dma fd520000.dma-controller: ZynqMP DMA driver Probe success
[ 6.272428] xilinx-zynqmp-dma fd530000.dma-controller: ZynqMP DMA driver Probe success
[ 6.280519] xilinx-zynqmp-dma fd540000.dma-controller: ZynqMP DMA driver Probe success
[ 6.288608] xilinx-zynqmp-dma fd550000.dma-controller: ZynqMP DMA driver Probe success
[ 6.296701] xilinx-zynqmp-dma fd560000.dma-controller: ZynqMP DMA driver Probe success
[ 6.304787] xilinx-zynqmp-dma fd570000.dma-controller: ZynqMP DMA driver Probe success
[ 6.312948] xilinx-zynqmp-dma ffa80000.dma-controller: ZynqMP DMA driver Probe success
[ 6.321037] xilinx-zynqmp-dma ffa90000.dma-controller: ZynqMP DMA driver Probe success
[ 6.329142] xilinx-zynqmp-dma ffaa0000.dma-controller: ZynqMP DMA driver Probe success
[ 6.337235] xilinx-zynqmp-dma ffab0000.dma-controller: ZynqMP DMA driver Probe success
[ 6.345327] xilinx-zynqmp-dma ffac0000.dma-controller: ZynqMP DMA driver Probe success
[ 6.353415] xilinx-zynqmp-dma ffad0000.dma-controller: ZynqMP DMA driver Probe success
[ 6.361503] xilinx-zynqmp-dma ffae0000.dma-controller: ZynqMP DMA driver Probe success
[ 6.369595] xilinx-zynqmp-dma ffaf0000.dma-controller: ZynqMP DMA driver Probe success
[ 6.378451] spi_master spi0: cannot find modalias for /axi/spi@ff0f0000/flash@0
[ 6.385767] spi_master spi0: Failed to create SPI device for /axi/spi@ff0f0000/flash@0
[ 6.393995] macb ff0c0000.ethernet: Not enabling partial store and forward
[ 6.403916] macb ff0c0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0c0000 irq 38 (70:b3:d5:9a:60:95)
[ 6.414129] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[ 6.420667] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[ 6.427167] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[ 6.433663] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[ 6.433695] zynqmp_pll_disable() clock disable failed for dpll_int, ret = -13
[ 6.467860] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 6.473356] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 6.481105] xhci-hcd xhci-hcd.1.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000002010090
[ 6.490514] xhci-hcd xhci-hcd.1.auto: irq 55, io mem 0xfe200000
[ 6.496637] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15
[ 6.504896] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 6.512116] usb usb1: Product: xHCI Host Controller
[ 6.516985] usb usb1: Manufacturer: Linux 5.15.36-xilinx-v2022.2 xhci-hcd
[ 6.523764] usb usb1: SerialNumber: xhci-hcd.1.auto
[ 6.528929] hub 1-0:1.0: USB hub found
[ 6.532704] hub 1-0:1.0: 1 port detected
[ 6.536812] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 6.542298] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 6.549965] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 6.556531] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 6.564738] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.15
[ 6.573000] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 6.580220] usb usb2: Product: xHCI Host Controller
[ 6.585088] usb usb2: Manufacturer: Linux 5.15.36-xilinx-v2022.2 xhci-hcd
[ 6.591868] usb usb2: SerialNumber: xhci-hcd.1.auto
[ 6.596976] hub 2-0:1.0: USB hub found
[ 6.600743] hub 2-0:1.0: 1 port detected
[ 6.605432] cdns-i2c ff020000.i2c: 90 kHz mmio ff020000 irq 40
[ 6.611667] i2c i2c-1: of_i2c: modalias failure on /axi/i2c@ff030000/i2c@1
[ 6.618545] i2c i2c-1: Failed to create I2C device for /axi/i2c@ff030000/i2c@1
[ 6.625771] cdns-i2c ff030000.i2c: 90 kHz mmio ff030000 irq 41
[ 6.635641] of_cfs_init
[ 6.638128] of_cfs_init: OK
[ 6.641037] clk: Not disabling unused clocks
[ 6.645563] ALSA device list:
[ 6.648518] No soundcards found.
[ 6.665271] mmc0: SDHCI controller on ff160000.mmc [ff160000.mmc] using ADMA 64-bit
[ 6.673470] Freeing unused kernel memory: 2176K
[ 6.678057] Run /init as init process
[ 6.691413] systemd[1]: System time before build time, advancing clock.
[ 6.701624] systemd[1]: systemd 249.7+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 6.731930] systemd[1]: Detected architecture arm64.
[ 6.747738] mmc0: new HS200 MMC card at address 0001
[ 6.753127] mmcblk0: mmc0:0001 DG4008 7.28 GiB
[ 6.758856] mmcblk0: p1 p2
Welcome to PetaLinux 2022.2_release_S10071807 (honister) 6.762058] mmcblk0boot0: mmc0:0001 DG4008 4.00 MiB
m!
[ 6.773141] mmcblk0boot1: mmc0:0001 DG4008 4.00 MiB
[ 6.778850] mmcblk0rpmb: mmc0:0001 DG4008 4.00 MiB, chardev (241:0)
[ 6.793226] systemd[1]: Hostname set to <PCIedemogem1demov1>.
[ 6.799098] systemd[1]: Initializing machine ID from random generator.
[ 6.832264] systemd-sysv-generator[233]: SysV service '/etc/init.d/watchdog-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 6.859175] systemd-sysv-generator[233]: SysV service '/etc/init.d/nfsserver' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 6.883203] systemd-sysv-generator[233]: SysV service '/etc/init.d/nfscommon' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 6.907488] systemd-sysv-generator[233]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 6.932529] systemd-sysv-generator[233]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 7.151202] systemd[1]: Queued start job for default target Multi-User System.
[ 7.186179] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty 7.197066] usb 1-1: new high-speed USB device number 2 using xhci-hcd
m.
[ 7.214407] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 7.238304] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 7.262145] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 7.285304] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 7.309251] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 7.333279] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 7.349141] systemd[1]: Reached target Remote File Systems.
[ 7.349806] usb 1-1: New USB device found, idVendor=0781, idProduct=558a, bcdDevice= 1.00
[ 7.362877] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 7.370009] usb 1-1: Product: Ultra
[ 7.373489] usb 1-1: Manufacturer: SanDisk
[ OK ] Reached target Remote File Systems usb 1-1: SerialNumber: 04010a68dc594b346ba446d43f720771d74295c42f90d1891398f98d49fdeb8f412b00000000000000000000eea67d39001665188a5581072c2c9749
[0m.
[ 7.397711] usb-storage 1-1:1.0: USB Mass Storage device detected
[ 7.404064] scsi host0: usb-storage 1-1:1.0
[ 7.417156] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 7.433156] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 7.449611] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 7.473130] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 7.493381] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 7.509281] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 7.533592] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 7.553343] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 7.573408] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 7.589554] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 7.613420] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 7.633332] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 7.653352] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 7.679599] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 7.699640] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 7.723768] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 7.741461] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[ 7.752473] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 7.769369] systemd[1]: Condition check resulted in Create List of Static Device Nodes being skipped.
[ 7.781527] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 7.800101] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 7.820008] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 7.839948] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 7.853215] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 7.862937] systemd[1]: Condition check resulted in Load Kernel Modules being skipped.
[ 7.873193] systemd[1]: Mounting NFSD configuration filesystem...
Mounting NFSD configuration filesystem...
[ 7.891862] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 7.915905] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 7.935914] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 7.957537] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 7.973636] systemd[1]: Mounted Huge Pages File System.
[ OK ] Mounted Huge Pages File System.
[ 7.993546] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 8.017565] systemd[1]: Mounted Kernel Debug File System.
[ OK ] Mounted Kernel Debug File System.
[ 8.037601] systemd[1]: Mounted Temporary Directory /tmp.
[ OK ] Mounted Temporary Directory /tmp.
[ 8.058133] systemd[1]: modprobe@configfs.service: Deactivated successfully.
[ 8.066459] systemd[1]: Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module configfs.
[ 8.090008] systemd[1]: modprobe@drm.service: Deactivated successfully.
[ 8.097797] systemd[1]: Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module drm.
[ 8.117800] systemd[1]: modprobe@fuse.service: Deactivated successfully.
[ 8.125685] systemd[1]: Finished Load Kernel Module fuse.
[ OK ] Finished Load Kernel Module fuse.
[ 8.145425] systemd[1]: proc-fs-nfsd.mount: Mount process exited, code=exited, status=32/n/a
[ 8.153909] systemd[1]: proc-fs-nfsd.mount: Failed with result 'exit-code'.
[ 8.162100] systemd[1]: Failed to mount NFSD configuration filesystem.
[FAILED] Failed to mount NFSD configuration filesystem.
See 'systemctl status proc-fs-nfsd.mount' for details.
[ 8.197126] systemd[1]: Dependency failed for NFS Mount Daemon.
[DEPEND] Dependency failed for NFS Mount Daemon.
[ 8.217096] systemd[1]: Dependency failed for NFS server and services.
[DEPEND] Dependency failed for NFS server and services.
[ 8.241091] systemd[1]: nfs-server.service: Job nfs-server.service/start failed with result 'dependency'.
[ 8.250685] systemd[1]: nfs-mountd.service: Job nfs-mountd.service/start failed with result 'dependency'.
[ 8.261799] systemd[1]: Finished Remount Root and Kernel File Systems.
[ OK ] Finished Remount Root and Kernel File Systems.
[ 8.286544] systemd[1]: Finished Apply Kernel Variables.
[ OK ] Finished Apply Kernel Variables.
[ 8.311743] systemd[1]: Condition check resulted in FUSE Control File System being skipped.
[ 8.323153] systemd[1]: Mounting Kernel Configuration File System...
Mounting Kernel Configuration File System...
[ 8.345387] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped.
[ 8.354029] systemd[1]: Condition check resulted in Platform Persistent Storage Archival being skipped.
[ 8.366558] systemd[1]: Starting Create System Users...
Starting Create System Users...
[ 8.384897] systemd[1]: Mounted Kernel Configuration File System.
[ OK ] Mounted Kernel Configuration File System.
[ 8.406982] systemd[1]: Finished Create System Users.
[ OK ] Finished Create System Users.
[ 8.412841] scsi 0:0:0:0: Direct-Access SanDisk Ultra 1.00 PQ: 0 ANSI: 6
[ 8.426957] sd 0:0:0:0: [sda] 60088320 512-byte logical blocks: (30.8 GB/28.7 GiB)
[ 8.437554] systemd[1]: Starting Create Static Device Nodes in /dev...
Starting Create Static Device Nodes in /dev[ 8.444487] sd 0:0:0:0: [sda] Write Protect is off
...
[ 8.455266] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
[ 8.467393] systemd[1]: Finished Create Static Device Nodes in /dev.
[ OK ] Finished Create Static Device Nodes in /dev.
[ 8.484902] sda: sda1
[ 8.488563] sd 0:0:0:0: [sda] Attached SCSI removable disk
[ 8.501445] systemd[1]: Reached target Preparation for Local File Systems.
[ OK ] Reached target Preparation for Local File Systems.
[ 8.527950] systemd[1]: Mounting /var/volatile...
Mounting /var/volatile...
[ 8.544772] systemd[1]: Started Entropy Daemon based on the HAVEGE algorithm.
[ OK ] Started Entropy Daemon based on the HAVEGE algorithm.
[ 8.569861] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 8.582767] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 8.594966] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 8.613427] systemd[1]: Starting Rule-based Manager for Device Events and Files...
Starting Rule-based Manage…for Device Events and Files...
[ 8.639387] systemd[1]: Mounted /var/volatile.
[ OK ] Mounted /var/volatile.
[ 8.655084] systemd[1]: Finished Coldplug All udev Devices.
[ OK ] Finished Coldplug All udev Devices.
[ 8.677556] systemd[1]: Condition check resulted in Bind mount volatile /var/cache being skipped.
[ 8.686600] systemd[1]: Condition check resulted in Bind mount volatile /var/lib being skipped.
[ 8.698388] systemd[1]: Starting Load/Save Random Seed...
Starting Load/Save Random Seed...
[ 8.713284] systemd[1]: Condition check resulted in Bind mount volatile /var/spool being skipped.
[ 8.724622] systemd[1]: Condition check resulted in Bind mount volatile /srv being skipped.
[ 8.738000] systemd[1]: Reached target Local File Systems.
[ OK ] Reached target Local File Systems.
[ 8.769555] systemd[1]: Starting Rebuild Dynamic Linker Cache...
Starting Rebuild Dynamic Linker Cache...
[ 8.787216] systemd[1]: Started Rule-based Manager for Device Events and Files.
[ OK ] Started Rule-based Manager for Device Events and Files.
[ 8.817738] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Finished Load/Save Random Seed.
[ OK ] Finished Rebuild Dynamic Linker Cache.
Starting Flush Journal to Persistent Storage...
[ 8.891359] systemd-journald[268]: Received client request to flush runtime journal.
Starting Network Configuration...
[ OK ] Finished Flush Journal to Persistent Storage.
Starting Create Volatile Files and Directories...
[ 8.957857] asmip: loading out-of-tree module taints kernel.
[ 8.963947] ASMIP.
[ 8.974271] asm_init: Registers mapped to mmio = 0x985d000
[ 8.979980] Registeration is a success the major device number is 0.
[ 8.986345] If you want to talk to the device driver,
[ 8.991409] create a device file by following command.
[ 8.991409]
[ 8.998200] mknod ASM c 0 0
[ 8.998200]
[ 9.002696] asm a0050000.ASM_IP_v3: Device Tree Probing
[ 9.007962] asm a0050000.ASM_IP_v3: no IRQ found
[ 9.012591] asm a0050000.ASM_IP_v3: asm at 0xa0050000 mapped to 0x0985f000
[ OK ] Finished Create Volatile Files and Directories.
Starting Rebuild Journal Catalog...
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Rebuild Journal Catalog.
Starting Update is Completed...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Finished Update is Completed.
[ OK ] Started Network Configuration.
Starting Network Name Resolution...
[ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Reached target Timer Units.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ OK ] Started Kernel Logging Service.
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.
Starting LSB: NFS support for both client and server...
Starting User Login Management...
[ OK ] Started LSB: NFS support for both client and server.
[ 10.145856] macb ff0c0000.ethernet eth0: PHY [ff0c0000.ethernet-ffffffff:00] driver [TI DP83867] (irq=POLL)
[ 10.155658] macb ff0c0000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 10.179299] pps pps0: new PPS source ptp0
[ 10.185543] macb ff0c0000.ethernet: gem-ptp-timer ptp clock registered.
[ OK ] Started Network Name Resolution.
[ OK ] Started User Login Management.
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting inetd.busybox.service...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting LSB: Kernel NFS server support...
Starting File System Check on /dev/mmcblk0p1...
Starting File System Check on /dev/mmcblk0p2...
Starting File System Check on /dev/sda1...
Starting Permit User Sessions...
Starting Target Communication Framework agent...
[ OK ] Started inetd.busybox.service.
[FAILED] Failed to start LSB: Kernel NFS server support.
See 'systemctl status nfsserver.service' for details.
[ OK ] Finished File System Check on /dev/mmcblk0p1.
[ OK ] Finished File System Check on /dev/mmcblk0p2.
[ OK ] Finished File System Check on /dev/sda1.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Target Communication Framework agent.
Mounting /run/media/mmcblk0p1...
Mounting /run/media/mmcblk0p2...
[ 11.507933] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
Mounting /run/media/sda1...
[ 11.535937] FAT-fs (mmcblk0p2): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyPS0.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
[ 11.616239] FAT-fs (sda1): Invalid FSINFO signature: 0x00000000, 0x00000000 (sector = 1)
[ 11.626761] FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
Starting Record Runlevel Change in UTMP...
[ OK ] Mounted /run/media/mmcblk0p1.
[ OK ] Mounted /run/media/mmcblk0p2.
[ OK ] Mounted /run/media/sda1.
[ OK ] Finished Record Runlevel Change in UTMP.
PetaLinux 2022.2_release_S10071807 PCIedemogem1demov1 ttyPS0
PCIedemogem1demov1 login: root
Password:
[ 34.465853] audit: type=1006 audit(1637342395.771:2): pid=673 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ 34.478157] audit: type=1300 audit(1637342395.771:2): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffec1e0b60 a2=1 a3=ffffb127d6b0 items=0 ppid=1 pid=673 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[ 34.504437] audit: type=1327 audit(1637342395.771:2): proctitle="(systemd)"
^Croot@PCIedemogem1demov1:~#
root@PCIedemogem1demov1:~#
root@PCIedemogem1demov1:~# ifconfig
eth0 Link encap:Ethernet HWaddr 70:B3:D5:9A:60:95
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:38
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:6 errors:0 dropped:0 overruns:0 frame:0
TX packets:6 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:400 (400.0 B) TX bytes:400 (400.0 B)
root@PCIedemogem1demov1:~# ifconfig eth0 192.168.10.120 up
root@PCIedemogem1demov1:~# ifconfig
eth0 Link encap:Ethernet HWaddr 70:B3:D5:9A:60:95
inet addr:192.168.10.120 Bcast:192.168.10.255 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:38
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:6 errors:0 dropped:0 overruns:0 frame:0
TX packets:6 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:400 (400.0 B) TX bytes:400 (400.0 B)
root@PCIedemogem1demov1:~#
root@PCIedemogem1demov1:~#
root@PCIedemogem1demov1:~# ping 192.168.10.12
PING 192.168.10.12 (192.168.10.12): 56 data bytes
^C
--- 192.168.10.12 ping statistics ---
7 packets transmitted, 0 packets received, 100% packet loss
root@PCIedemogem1demov1:~#
root@PCIedemogem1demov1:~# ping 192.168.10.120
PING 192.168.10.120 (192.168.10.120): 56 data bytes
64 bytes from 192.168.10.120: seq=0 ttl=64 time=0.091 ms
64 bytes from 192.168.10.120: seq=1 ttl=64 time=0.051 ms
64 bytes from 192.168.10.120: seq=2 ttl=64 time=0.045 ms
64 bytes from 192.168.10.120: seq=3 ttl=64 time=0.043 ms
^C
--- 192.168.10.120 ping statistics ---
4 packets transmitted, 4 packets received, 0% packet loss
round-trip min/avg/max = 0.043/0.057/0.091 ms
root@PCIedemogem1demov1:~#
root@PCIedemogem1demov1:~#
Please help.