Part Number: DP83826I
Other Parts Discussed in Thread: DP83826E
We are using the DP83826I in Basic mode, and without a pull-down strap on the Duplex pin (RXD0 / pin16) the device only advertises 10/100 HD. With a pull-down fitted it advertises all modes 10/100, HD/FD, as expected. This is different to the KSZ8081 device that it's supposed to be compatible with. The datasheet description isn't particularly clear on this for register 0 and 4.
Can you clarify if this is the expected operation, as our expectations were that the speed and duplex settings only affect forced mode operation rather than autonegotiation, and in any case we expected same operation as the KSZ8081. The System Rollover document for the DP83826E also implies that there is no change required.