Part Number: TUSB1104EVM
Hi ,
The customer has the following problems when using EVM test, please help to answer them.
Question 1: If JMP 3 and 4 are set to automatic AEQ, the configuration options of JMP9 and JMP10 are invalid?
Question2: If only one data channel is connected, for example, the hard disk is connected to CRX1 and CTX1, JMP3 needs to short-circuit 3 and 4 to make CRX1-> SSRX1 and SSTX1-> Is CTX1 a configuration channel?
On the contrary, when connected to CRX2 and CTX2, JMP3 needs to short-circuit 1 and 2 to make CRX2-> SSRX2 and SSTX2-> Is CTX2 a configuration channel?
Question 3:
The customer's test environment:
1). Notebook Lightning 4 interface + typeC data cable 1 + TUSB1104EVM + typeC data cable 2 + solid state mobile hard drive;
2). The mobile hard disk can reach 10Gbps by connecting the lightning interface with typeC data cable 1 alone;
3).typeC data line 2 does not contain high-speed Tx2 difference line and Rx2 difference line, which is a single channel data line;
If the typeC data cable 2 is connected to the hard disk and there is an impedance change in the middle of this path, can TUSB1104EVM make the whole path reach 10Gbps by adjusting the balance parameters?
Thanks~