Part Number: MAX3232
Hello, I want to use the MAX3232 I.C. in order to use two different RS232 peripherals to communicate with a STM32 mcu. One of the peripherals has a baud rate of 9600Bps and the other has 115200Bps. Can I use both peripherals in the same MAX3232? Or are the 2 extra channels used only for CTS/RTS communication?