This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB319-Q1:Help. PD not active. only 500mA (ID Pin is normal)

Part Number: TUSB319-Q1
Other Parts Discussed in Thread: TPS54531, TPS25762-Q1, TPS25751

Hello
PCB was manufactured using TUSB319.
However, with only 500mA, USB PD doesn't work.


- 5VB+ and 5V BUS = power supply (5V/MAX20A) input.
- ID pin is good.
- U2 = 3A, Switch IC (active low)

I'm sending it with the PCB image and SCH.

What's the problem? T^T..

 1007.Question.pdf