Part Number: DP83TC811R-Q1
Other Parts Discussed in Thread: DP83TC811
Hi Team,
PHY_AD[3:0] configured by Boot strap cannot be accessed correctly.
Is there any possible reason?
<Details>
RX_ER(pin-14) and RX_DV(pin-15) are opened.
According to Table 17, it is Mode 1 in this case.
According to Table 18, PHY_AD[3:0]=0000b at Mode 1.
However, there is no response when accessing with 0000b.
Instead, when they accessed it with 0001b, they got a response.
The settings and behavior do not match.
Please let me know if there is a possible reason.
Best Regards,