Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Hello Support team,
For I210 IT(COPPER) to DP83869(FIBER) application, how to set the indicating LED(1G/100M/Link)?
(DP83869: LED_0, LED_1, LED_2 PINs)
Thanks.
Best Regards,
Dave
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dave,
What is the device mode being used (OP_MODE = 'xxx')? If RGMII to Copper is being used ('000'), are these default LED functions acceptable:

If not, the LED functions can be individually adjusted in register 18h.
For LED_0, set 0x18[3:0] = '1001' for indicating 100/1000BT link up. Similar adjustment is made in [11:8] and [7:4] for LED_2 / LED_1.
Thank you,
Evan