Part Number: SN65DSI83-Q1
Other Parts Discussed in Thread: DS90UH941AS-Q1
I am using the TI IC "SN65DSI83-Q1" for converting the MIPI-DSI to LVDS.
This IC is supporting 1.8V.
I want one IC which can convert this LVDS (1.8V) to 24-Bit Parallel Data.
At present I have DS90CF384MTD_NOPB which is 3.3V compatible. I can't interface this 3.3V LVDS IC with 1.8V LVDS output.