Part Number: SN65DP149
Hi,
I have the exact same problem as the refering question using the SN65DP149.
The SN65DP149 is connected to a DDI port of a ComExpress type 6.
+/- 5s after booting, when the DVI cable (desktop screen) is already connected, an I2C trame is sent from the ComExpress (I2C SRC = I2C 3V3) but not copied into I2C SNK (I2C 5V) :

When the cable is disconnected and reconnected, it works (SDA SRC is in 2nd position in this one to simplify debugging) :

The schematics is derived from the datasheet :



I've tried to force the HDP SRC to HIGH, did not change anything.
Does anyone have any idea?
Thanks !