Part Number: SN65DSI84
Other Parts Discussed in Thread: SN65DSI85
Hello,
We are using SN65DSI84 to convert from DSI to LVDS on our custom i.MX8MP board.
We used the DSI tunner to obtain the values for CSR registers, Our requirement is single channel DSI to single link LVDS (with 1 Clock & 4 Data lane), 24 BPP, and RGB888 Format. Instead of pannel we have an FPGA, i.MX8MP -> SN65DSI84 -> FPGA.
The issue is blank screen with some noise and we notice that LVDS clock frequency is very low (12.4MHz) when probed using oscilloscope instead of (actual 74.5MHz) and the PLL status bit in register 0x0A keeps changing, increasing the wait time for PLL lock did not work.
root@:~$ i2cget -f -y 1 0x2c 0x0a
0x8b
root@:~$ i2cget -f -y 1 0x2c 0x0a
0x0b
root@:~$ i2cget -f -y 1 0x2c 0x0a
0x8b
root@:~$ i2cget -f -y 1 0x2c 0x0a
0x0b
We need 1920x1080 resolution at 30 FPS at the bridge output & the timing info are mentioned below and also please find the attached screenshot of DSI tunner inputs.
Horizontal Timings:
HFP 88
HPW 44,
HBP 148,
Blanking Total 280,
Total Pixels 2200
Vertical Timings:
VFP 4,
VPW 5,
VBP 36,
Blanking Total 45
Total Lines 1125



Thanks & regards,
Shaswath