Part Number: TS3USBCA4
hi,
I have this MUX used for MUX AUX, SBU and LSX signals to SBU of USB connector.
May i know do i need pull up/down resistor for all those line ?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3USBCA4
hi,
I have this MUX used for MUX AUX, SBU and LSX signals to SBU of USB connector.
May i know do i need pull up/down resistor for all those line ?

Hi Woon:
Is this for source application of .sink application?
Regards
Brian
HI Woon:
MUX can left open if the channel is not used.
DP can be either source application or sink application, but can't not be both source and sink in the same application.
Can you also explain LSX signal ?
Here is the PU/PD for DP source application.

Regards
Brian
I assigned the ticket to PD controller group to see if ac cap is needed for LSX.
Regards
Brian
here is the updated design:
we used this for source application.
for LSX side, we have 0ohm resistor stuffing at level shifter side.
for pin 7 &8, it is either from AUX or HDMI_DDC signals.
Thanks Brian helping in checking.